Technical FAQs

Ask a Question

What is the replacement drive part number for a 3 HP VT drive unit @ 480 Volt?

The replacement VFD is the ATV61HU22N4.  
If the VFD is used in an M FLEX, E FLEX, 18 pluse or an MCC, the replacement VFD is the ATV61HU15N4 the power ID will need to be changed to IP00

CTA-ID : 2061831
Was this helpful?
What can we do to improve the information ?