Technical FAQs

Ask a Question

Can the 5.2E, 5.3E, 6.2E and 6.3E trip units handle dielectric (hi-pot)testing or should they be removed from the breaker prior to testing. Do wehave any documentation to state the proper procedure as we do with thePower & Harmonic trip units?

Bulletin 48940-313-01 page 85 states that Micrologic trip units can be left connected, even if equipped with voltage measurement (ENVT option).


CTA-ID : 2061833
Was this helpful?
What can we do to improve the information ?