Technical FAQs

Ask a Question

What are the dimensions and weight for the ATV61HD30N4 and ATV61HD37N4 drives?

Dimensions are weights are shown in the Installation manual.  

Both these drives are Frame size 7A.  The dimensions in inches are 9.45 (W), 21.65 (H), 10.47 (D) inches.  Note that the depth dimension does not include any option cards.  Up to two option cards can be added to each drive.  The weight is 81.57 pounds.  

CTA-ID : 2061778
Was this helpful?
What can we do to improve the information ?