Technical FAQs

Ask a Question

How many spaces are required for a QO2125 or QOB2125 breaker?

2 spaces are required.  Also,  there is a 40A maximum allowed to be mounted across from a 125A branch breaker.  Space the circuits accordingly.  




CTA-ID : 2061824
Was this helpful?
What can we do to improve the information ?