Technical FAQs

Ask a Question

What is the part number for the cooling fan for the ATV61HD90N4?

This drive has two fans - an Internal Cooling Fan and a Heatsink Fan.  

The Internal Cooling Fan is VZ3V1214.  This single fan located to the left of the control board and measures 3.14 by 3.14 inches.  This fan comes as part of a kit and there is one internal cooling fan per drive.

The Heatsink cooling fan is VZ2V1215.  This is a set of three fans each measuring 3.62 by 3.62 inches that mounts at the bottom of the drive.  The fans are not sold individually, it comes as part of the kit only.  Use one kit per drive.  


CTA-ID : 2061574
Was this helpful?
What can we do to improve the information ?