Technical FAQs

Ask a Question

What is the part number for the Main Control Board for the ATV58 TRX drives?

The part number is VX4A581U which is obsolete.
ATV58 Type E, F, N and H= VX4A581U  up to 75HP  (HD79).   This does not apply to the C10 thru C33 Drives.

The control board part number is VX4A381 for the HIgh HP ATV58 drives ATV58HC10N4 thru ATV59HC33N4 is also obsolete.
Both Main control boards are obsolete.
Was this helpful?
What can we do to improve the information ?