Technical FAQs

Ask a Question

S-Flex. Is there a way to reduce the motor speed when running in bypass?

On the S-Flex enclosed drives an across the line, IEC type, starter is used for bypass.  This only allows full speed operation.  


CTA-ID : 2061634
Was this helpful?
What can we do to improve the information ?