Technical FAQs

Ask a Question

How many analog inputs and analog outputs are in the standard ATV61/ATV71 drive?

The standard ATV61 and ATV71 has 2 analog inputs and 1 analog output.

If additional analog inputs/outputs are needed add the Extended I/O Option card part number VW3A3202.  This card would provide 2 more analog inputs and 2 more analog outputs.  


CTA-ID : 2061461
Was this helpful?
What can we do to improve the information ?