Technical FAQs

Ask a Question

What is the AIC rating for the HOM2150 main circuit breaker that works in the older series load centers?

The Short Circuit Current Rating is 10kA @ 120/240 Vac.


CTA-ID : 2061806
Was this helpful?
What can we do to improve the information ?