Technical FAQs

Ask a Question

What is the replacement fan for the ATV312HD15S6?

Issue:
Customer needs a replacement fan for the ATV312HD15S6.

Product Line:
ATV312

Environment:
ATV312HD15S6 - all versions

Cause:
Fan needs replaced

Resolution:
The fan kit is VZ3V3104.  
The kit contains two fans.  
Individual fans are not available, order the complete kit only.  


 
Was this helpful?
What can we do to improve the information ?