Technical FAQs

Ask a Question

ATV61. Can I set the R1 relay for both Drive Run and Drive Fault at the same time?

No, only one function can be assigned at a time to the Relay outputs.  


CTA-ID : 2061623
Was this helpful?
What can we do to improve the information ?