Technical FAQs

Ask a Question

Are metal legend plates available for the ZB4/ZB5 operators?

Issue:
Can’t locate metal legends for ZB4/ZB5 operators.

Product Line:
22mm Push Buttons ZB4/ZB5

Environment:
XB4 and XB5 operators.

Cause:
A metal legend plate is being called out for an application. 

Resolution:
Schneider Electric does not offer a 22mm metal legend plate at this time.   
 
Was this helpful?
What can we do to improve the information ?