Technical FAQs

Ask a Question

Do the XD4PA** Joysticks include the contact blocks?

Issue:
Do the XD4PA** Joysticks include the contact blocks?
Product Line:
XB4 Joysticks operators                
Environment:
22mm Push Buttons
Cause:
To determine if contacts need to be ordered separately.
Resolution:
Yes, contact blocks are included.
 
Was this helpful?
What can we do to improve the information ?