Technical FAQs

Ask a Question

Can the ATV12 command controls be split between HMI and terminals? Can the start / stop be commanded via the logic inputs and the forward / reverse be commanded via the HMI ?

This is not a feature of the ATV12 drive.

CTA-ID : 2061394
Was this helpful?
What can we do to improve the information ?