Technical FAQs

Ask a Question

What does the 9001SKY302 consist of?

Issue:
What does the 9001SKY302 consist of?

Product Line:
Push Buttons

Environment:
30mm Pushbuttons

Cause:

Resolution:




The 9001SKY302 consists of:
(1) 9001SKY3 enclosure, ((2) 9001SKR1B operators, (1) 9001SKR3R operator, (2) 9001KA1 contact blocks, (1) 9001KA3 contact block, (1) 9001KN111WP UP legend plate, (1) 9001KN110WP DOWN legend plate, and (1) 9001KN102RP STOP legend plate.


CTA-ID : 2061576
Was this helpful?
What can we do to improve the information ?