Technical FAQs

Ask a Question

Is the 9001SKY303 considered a momentary or maintained control station?

The 9001SKY303 consist of the (2) 9001SKR1B and (1) 9001SKR3R which are non-illuminated momentary push button operators.



CTA-ID : 2061226
Was this helpful?
What can we do to improve the information ?