Technical FAQs

Ask a Question

What is part number for a pilot light in a XACA pendant station?

Issue:
What is part number for a pilot light in a XACA pendant station?

Product Line:
Harmony Pendant Stations

Environment:
All Products

Cause:
Product Selection

Resolution:
Use any ZA2BV*** pilot light head and a
ZB2BV006 direct supply light module (without lamp for 6-120vac/dc applications) or
ZB2BV007 resistor base (with 130v lamp for 220-240vac/dc applications) .
Use DL1CE***  incandescent lamps , DL1CJUS***  LED lamps or NE51HRT***  neon lamps .


CTA-ID : 2061059
Was this helpful?
What can we do to improve the information ?