Technical FAQs

Ask a Question

What are the components that make up the 9001KYK14?

Issue:
What are the components that make up the 9001KYK14?

Product Line:
30mm Push

Environment:
9001K/SK/KX Push Buttons

Cause:
Part number is out of stock and needs to be ordered in parts.                                                      

Resolution:                                                                 
9001KY1 enclosure, 9001KR4R momentary mushroom button, 9001KA1 1 normally open and 1 normally closed contact block and 9001KN202 Stop legend plate.
 
Was this helpful?
What can we do to improve the information ?