Technical FAQs

Ask a Question

What is the force required to operate the 9001 P1 palm button?

2.02 pounds to actuate the first contact.  4.51 to actuate the second contact and 8.8 pounds to end of travel.
THE 9001 PALM BUTTONS ARE OBSOLETE


CTA-ID : 2061359
Was this helpful?
What can we do to improve the information ?