Technical FAQs

Ask a Question

What is the part number for the cooling fan for the ATV61HD11N4?

VZ3V1210 is the heatsink fan kit.  The kit comes with a small fan measuring 2.3 by 1 inches and a large fan measuring 3.14 by 1.5 inches.  Individual fans are not available, order the complete kit.  This drive uses one fan kit per drive.  


CTA-ID : 2061546
Was this helpful?
What can we do to improve the information ?