Technical FAQs

Ask a Question

What is the part number for the cooling fan for the ATV71HU30M3?

VZ3V1209 is the heatsink fan kit.  Each fan measures 2.3 by 2.3 inches.  A single fan is not available, order the complete kit.  The kit contains two fans and this drive uses one fan kit per drive.  


CTA-ID : 2061537
Was this helpful?
What can we do to improve the information ?