Technical FAQs

Ask a Question

What are the repair parts for a H92442, Series E2 Double throw Safety Switch?

The parts listed here are the only field replaceable parts.
Blade assembly - 40538-424-50
Top switch base assembly - 40538-425-50
Bottom switch base assembly - 40538-426-50  (Obsolete, No Longer Available)
Arc suppressor assembly - 40538-472-50
Handle knob assembly - 114930  (Obsolete - replaced by 40284-357-50)
Lug assembly - 40251-016-52
base mounting screws - 21427-171-61


CTA-ID : 2061674
Was this helpful?
What can we do to improve the information ?