Technical FAQs

Ask a Question

How can I set an ATV61 or ATV71 for HMI speed reference and terminals for start/ stop controls?

1.6 Command menu
Set ref ch 1  to HMI
Set Profile to separate
CMD switching =channel 1 active
CMD channel = Terminal control
1.7 Application Function menu
Set ref 1B switch to ch1 active

Now you can start the drive with LI1 and +24vdc 2 wire control and use the HMI knob as the speed reference.


CTA-ID : 2061336
Was this helpful?
What can we do to improve the information ?