Technical FAQs

Ask a Question

What are the replacement contact blocks for the 9001P5 palm button?

Part number 31013-051-51 is a sealed assembly of a bracket, (2) 9001KA2 and (2) 9001KA3.  The contact blocks must be replaced only as this complete assembly.

REVISED 11/9/2012 - Although the contact block is still available, the 9001P5 palm button is obsolete.
Was this helpful?
What can we do to improve the information ?