Technical FAQs

Ask a Question

What is the part number for the cooling fan for the ATV71HD30N4?

VZ3V1206 is the heatsink fan kit.  The fans measure 3.62 by 3.62 inches each.  The kit contains two fans and this drive uses one fan kit per drive.  The fans are not available individually, it is only available as a kit.  


CTA-ID : 2061521
Was this helpful?
What can we do to improve the information ?