Technical FAQs

Ask a Question

What is the part number for the cooling fan for the ATV71HD45M3X?

VZ3V1207 is the heatsink fan kit.  Each fan measures 3.62 by 3.62 inches.  A single fan is not available, order the complete kit.  The kit contains two fans and this drive uses one fan kit per drive.  

CTA-ID : 2061525
Was this helpful?
What can we do to improve the information ?