Technical FAQs

Ask a Question

What is the part number for the cooling fan for the ATV61HD37M3X?

VZ3V1207 is the heat sink fan kit.  Each fan measures 3.62 by 3.62 inches.  A single fan is not available, order the complete kit.  The kit contains two fans and this drive uses one fan kit per drive. 
Was this helpful?
What can we do to improve the information ?