Technical FAQs

Ask a Question

What are the part numbers for early closing and late opening contacts for a 9001K, 9001SK, 9001KX, or 9001T operators?

9001KA5 is a normally closed late opening contact and a 9001KA6 is a normally open early closing contact.  These can be used together to provide overlapping contacts.


CTA-ID : 2061321
Was this helpful?
What can we do to improve the information ?