Technical FAQs

Ask a Question

When programming the ATS48 analog output for motor current, AO=OCr, is the scaling parameter ASC a percentage based on the motor current parameter In or based on the nameplate current rating of the specific ATS48?

It is based on the motor current programmed into In.  It is adjustable from 50 to 500% of the In value.

CTA-ID : 2061349
Was this helpful?
What can we do to improve the information ?