Technical FAQs

Ask a Question

On an ATS48, how is the R1 relay set to function as a fault relay?

From the display status screen, typically rdY or nLP, arrow down to the IO menu and ENT.  Arrow to parameter r1, ENT and change to R1F. ENT to save.

CTA-ID : 2061612
Was this helpful?
What can we do to improve the information ?