Technical FAQs

Ask a Question

If the Generator kit HOMCRBGK1 is installed in the correct load center with Utility power OFF and Generator ON, will the LC MB automatically turn ON if or when Utility power is restored?

Product Design Features

Product Line:
Homeline load centers

Generator kits

Understanding the operation


NO, the HOMCRBGK1 is a MANUALLY operated generator interlock kit, which restricts the load center main breaker from being ON while the generator breaker is ON and requires the generator breaker to physically be turned OFF before the Load Center main breaker can be turned ON.

CTA-ID : 2061452
Was this helpful?
What can we do to improve the information ?