Technical FAQs

Ask a Question

How do you turn off the torque control in the ATS22 softstarts?

Under the ConF menu scroll to parameter LAC, push the ENT button.  Change from oFF to On.  Push ENT button to save.  
Next, go to the AdJ menu and scroll to paramterr SSC.  Change SSC to oFF.  Push ENT button to save.  
When finished, push the ESC button until you see rdY, nrdY or rUn

CTA-ID : 2061456
Was this helpful?
What can we do to improve the information ?