Technical FAQs

Ask a Question

Can the flush cover for the J250F Series A01 enclosure be converted to a surface cover?

Issue:
Product Design features

Product Line:
Circuit Breaker Enclosures

Environment:
Cover conversion

Cause:
Application

Resolution:
The J250F Series A01 flush cover can be replaced with a surface cover, part number J250SC.
NOTE: The J250F can actually be mounted in a surface application with the standard Flush cover, but the cover will Overhang the enclosure a small amount completely around the enclosure.


CTA-ID : 2061580
Was this helpful?
What can we do to improve the information ?