Technical FAQs

Ask a Question

What are the overall dimensions of the Q22200NS enclosures?

Issue:
Product Characteristics

Product Line:
CB Enclosure

Cause:
Dimensions

Resolution:
The Q22200NS is 23,12" H x 7.56" W x 4.25" D.


CTA-ID : 2061410
Was this helpful?
What can we do to improve the information ?