Technical FAQs

Ask a Question

What is the load or line reactor that can be used with an ATV71HU75N4 Drive?

A 5% reactor is part number RL01803 for open style.  This is also available in a NEMA 1 enclosure, part number RL01813.  These reactors can be used on the line or load side of any 10HP, 460V rated AC drive.  

CTA-ID : 2061245
Was this helpful?
What can we do to improve the information ?