Technical FAQs

Ask a Question

Are NQ panels ABS rated?

Are NQ panelboards ABS rated?

Product Line:
PTFDS - FD Enclosure Systems

NQ panelboards sold and supported in the USA.

Does the NQ line of panelboards meet the American Bureau of Shipping Standards?

NQ panels meet American Bureau of Shipping Standards (ABS) for steel vessels 2010 .
The certification was renewed in 2015 and runs through 2020.

To view the certification on the ABS website, go to the site below and search for "panelboard"

CTA-ID : 2058972
Was this helpful?
What can we do to improve the information ?