Technical FAQs

Ask a Question

Can I use the ATV61/71 HMI keypad, part number VW3A1101, on a Altivar 31 drive?

No.  The ATV61 / 71 keypad can be used on the ATV312 drives, but not on the ATV31 drives.  See remote keypad part number VW3A31101 for the ATV31 drives.


CTA-ID : 2061329
Was this helpful?
What can we do to improve the information ?