Technical FAQs

Ask a Question

What does the motor Thermal state indicate on the ATV66 keypad display?

It is a percentage from 0-200%, 100% will cause the yellow LED, on the faceplate of the drive to blink, as an early warning signal. When the thermal state reaches 118%, the drive will trip on Motor Overload Fault.

CTA-ID : 2061428
Was this helpful?
What can we do to improve the information ?