Technical FAQs

Ask a Question

What is the part number for a blank cover to cover the opening for a QBL type breaker removed from a NQ interior using a NQMB2Qmain breaker adapter kit?

Issue:
What is the part number for a blank cover to cover the opening for a QBL type breaker removed from a NQ interior using a NQMB2Qmain breaker adapter kit?


Product Line:
PTFDS - FD Enclosure Systems


Environment:
NQ panelboards and accessories sold and supported in the USA.


Cause:
Replacement blank cover when removing the QBL main from an NQ interior.


Resolution:
The blank cover part number is 80116-270-01. Installation will also require (2) 24303-63190 mounting rivets.  










CTA-ID : 2057645
Was this helpful?
What can we do to improve the information ?