Technical FAQs

Ask a Question

What is the difference between the ATV31HD11N4 and ATV31CD11N4?

The ATV31HD11N4 is IP00 rated and the ATV31CD11N4 is IP54 rated.  IP00 enclosure rating is considered Open type.  IP54 is similar to a NEMA 12 enclosed rating .  


CTA-ID : 2061064
Was this helpful?
What can we do to improve the information ?