Technical FAQs

Ask a Question

When is a plug-on extension needed for a QMB363T ?

Use this assembly if the bus is flatwise, the panel or switchboard section is 38`w (or wider ) and the panel or switchboard section is labeled QW.


CTA-ID : 2054576
Was this helpful?
What can we do to improve the information ?