Technical FAQs

Ask a Question

Can the ATV66 standard drive accept an encoder feedback?

No, but you can use a converter to convert the encoder signal to a 0-10V or 4-20 (0-20) ma and use it to control the speed.

CTA-ID : 2061425
Was this helpful?
What can we do to improve the information ?