Technical FAQs

Ask a Question

Can you program the Altivar ATV66 unit with single phase power and it retain the memory?

Need to remove the jumpers on CL1 to L1 and CL2 to L2.    Then power up CL1 and CL2 only.    This will allow  the programming be saved.

CTA-ID : 2061421
Was this helpful?
What can we do to improve the information ?