Technical FAQs

Ask a Question

Do we have any drives that have flux vector control?

Yes, while the majority of our drives have sensorless flux vector control, we do have  ATV66, ATV58 and ATV71 drives, that are flux vector controlled. The Flux Vector control uses encoder feedback. Only ATV71 is currently available. ATV66 and ATV58 are obsolete.


CTA-ID : 2061420
Was this helpful?
What can we do to improve the information ?