Technical FAQs

Ask a Question

Is a Flush mounted stainless steel enclosure like the FA100DS available?

Issue:
Product design features

Product line:
Circuit breaker enclosure

Environment:
Locking features

Cause:
Application

Resolution:
No, the stainless steel enclosures are only available as a surface mount.


 
Was this helpful?
What can we do to improve the information ?