Technical FAQs

Ask a Question

What are the repair parts for a QO130L200GRB, Series S1, Load Center?

Only the parts listed below are considered field replaceable.
Cover - 4054802204 (The cover is OBSOLETE, NO LONGER AVAILABLE WITH NO REPLACEMENT)
Interior Trim - 4054520301
Interior Assembly - QO130L200GRBI
Neutral Bonding Screw - 4028344850K
Main Lugs - QOL225
Interior trim mounting screw - 4020513001K
RB door mounting screw - 2142717161
Main circuit breaker and main lugs keps nut - 2342702001


CTA-ID : 2061293
Was this helpful?
What can we do to improve the information ?