Technical FAQs

Ask a Question

Are the 9007 type CR Limit Switches rated Nema 7 and 9?

Yes, they are rated Nema 7 & Nema 9 for explosion proof applications.  Its also rated for NEMA 1, 2, 4, 6, 6P, 7, 9, 12 and 13 rated.


CTA-ID : 2061114
Was this helpful?
What can we do to improve the information ?