Technical FAQs

Ask a Question

Can you replace the LCD display unit on H, J or L Powerpact breakers with the Micrologic 5 or 6 Trip units?

Issue:
Can you replace the LCD display unit on H, J or L Powerpact breakers with the Micrologic 5  or 6  Trip units?

Product Line:
Powerpact H, J and L

Environment:
Micrologic Trip Unit

Cause:
Display is blank when fully powered up.

Resolution:
Yes.
For Micrologic 5 trip units use S429483
For Micrologic 6 trip units use S429484


CTA-ID : 2061156
Was this helpful?
What can we do to improve the information ?