Technical FAQs

Ask a Question

Are Compact NSE breakers such as NENL34090 still available?

All Compact NSE breakers are obsolete and have been replaced with the Powerpact HD type breakers.  Note that the HD breakers are larger in size and may not fit in the same space as the NSE.

CTA-ID : 2061195
Was this helpful?
What can we do to improve the information ?