Technical FAQs

Ask a Question

What does the SE code mean on the VSD07 drive display?

SE means Serial control.  The optional remote keypad is active as the user interface instead of the buttons on the front of the drive.  

CTA-ID : 2061249
Was this helpful?
What can we do to improve the information ?